This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用超级终端登陆nfs挂载板子的时候,打印出VBUS_ERR的错误,USB鼠标无法使用。打印信息如下:
----------------------------------------------------------------------------------------------------------------------------------------
U-Boot 1.2.0 (Feb 12 2009 - 16:54:02)
dram_init info:
start:0x80000000, size:0x8000000
DRAM: 128 MB
NAND: 64 MB
In: serial
Out: serial
Err: serial
ARM Clock : 297MHz
DDR Clock : 135MHz
ETH PHY : BroadCom PHY Chip
Hit any key to stop autoboot: 0
Loading from NAND 64MiB 1,8V 8-bit, offset 0x168000
Image Name: Linux-2.6.10_mvl401-davinci_evm
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1580956 Bytes = 1.5 MB
Load Address: 80008000
Entry Point: 80008000
Automatic boot of image at addr 0x80800000 ...
## Booting image at 80800000 ...
Image Name: Linux-2.6.10_mvl401-davinci_evm
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1580956 Bytes = 1.5 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
OK
Starting kernel ...
Uncompressing Linux............................................................. Linux version 2.6.10_mvl401-davinci_evm (root@localhost.localdomain) (gcc versio n 3.4.3 (MontaVista 3.4.3-25.0.30.0501131 2005-07-23)) #46 Thu Oct 23 04:34:17 E DT 2008
CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists
Kernel command line: mem=60M console=ttyS0,115200n8 root=/dev/nfs noinitrd rw ip =192.168.1.197:255.255.255.0:192.168.1.1 nfsroot=192.168.1.196:/opt/nfs video=dm 64xxfb:output=pal
PID hash table entries: 256 (order: 8, 4096 bytes)
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 60MB = 60MB total
Memory: 57472KB available (2577K code, 629K data, 144K init)
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
spawn_desched_task(00000000)
desched cpu_callback 3/00000000
ksoftirqd started up.
desched cpu_callback 2/00000000
desched thread 0 started up.
NET: Registered protocol family 16
Registering platform device 'nor_davinci.0'. Parent at platform
Registering platform device 'nand_davinci.0'. Parent at platform
Registering platform device 'musb_hdrc'. Parent at platform
DaVinci I2C DEBUG: 12:14:45 May 16 2008
Registering platform device 'i2c'. Parent at platform
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NTFS driver 2.1.22 [Flags: R/W].
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
yaffs May 16 2008 12:14:06 Installing.
Registering platform device 'davincifb.0'. Parent at platform
Console: switching to colour frame buffer device 90x36
Registering platform device 'davinci_resizer.2'. Parent at platform
Registering platform device 'davinci_previewer.2'. Parent at platform
Registering platform device 'davinci_pwm0.0'. Parent at platform
Registering platform device 'davinci_pwm1.1'. Parent at platform
Registering platform device 'davinci_pwm2.2'. Parent at platform
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
Registering platform device 'serial8250'. Parent at platform
ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
ttyS1 at MMIO 0x1c20400 (irq = 41) is a 16550A
io scheduler noop registered
io scheduler anticipatory registered
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Registering platform device 'ti_davinci_emac'. Parent at platform
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
netconsole: not configured, aborting
i2c /dev entries driver
Linux video capture interface: v1.00
Registering platform device 'vpfe.1'. Parent at platform
TVP5150 support for SEED_DVS6446 by Stephen Zhang
DaVinci v4l2 capture driver V1.0 loaded
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
hda: CSD CAV040H, ATA DISK drive
elevator: using anticipatory as default io scheduler
ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22
hda: max request size: 128KiB
hda: 78140160 sectors (40007 MB) w/8192KiB Cache, CHS=65535/16/63
hda: hda1 hda2
ide0: BM-DMA at 0xe1066000-0xe1066007, BIOS settings: hda:pio, hdb:pio
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.0:USB HID core driver
mice: PS/2 mouse device common for all mice
musb_hdrc: version 2.2a/db-0.4.8 [pio] [host] [debug=0]
musb_hdrc: USB Host mode controller at c4060000 using PIO, IRQ 12
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Registering platform device 'mmc0.1'. Parent at platform
: Supporting 4-bit mode
VBUS_ERR
Registering platform device 'davinci-audio.0'. Parent at platform
DAVINCI AIC23 audio support initialized
NET: Registered protocol family 2
IP: routing cache hash table of 512 buckets, 4Kbytes
TCP: Hash tables configured (established 4096 bind 8192)
NET: Registered protocol family 1
NET: Registered protocol family 17
IP-Config: Guessing netmask 255.255.255.0
IP-Config: Complete:
device=eth0, addr=192.168.1.197, mask=255.255.255.0, gw=192.168.1.1,
host=192.168.1.197, domain=, nis-domain=(none),
bootserver=255.255.255.0, rootserver=192.168.1.196, rootpath=
Looking up port of RPC 100003/2 on 192.168.1.196
Looking up port of RPC 100005/1 on 192.168.1.196
VFS: Mounted root (nfs filesystem).
Freeing init memory: 144K
INIT: version 2.85 booting
Mounting a tmpfs over /dev...done.
Creating initial device nodes...done.
Activating swap...done.
Remounting root filesystem...done.
Calculating module dependencies
WARNING: Couldn't open directory /lib/modules/2.6.10_mvl401-davinci_evm: No such file or directory
FATAL: Could not open /lib/modules/2.6.10_mvl401-davinci_evm/modules.dep.temp for writing: No such file or directory
Loading modules:
Starting checking all file systems: fsck
fsck 1.35 (28-Feb-2004)
Starting mounting local filesystems: mount nothing was mounted
Cleaning: /etc/network/ifstate.
Setting up IP spoofing protection: rp_filter.
Disable TCP/IP Explicit Congestion Notification: done.
Starting network interfaces: done.
Starting hotplug subsystem:
pci
pci [success]
usb
usb [success]
isapnp
isapnp [success]
ide
ide [success]
input
input [success]
scsi
scsi [success]
done.
Starting portmap daemon: portmap.
Cleaning: /tmp /var/lock /var/run done.
Setting pseudo-terminal access permissions...done.
Updating /etc/motd...done.
INIT: Entering runlevel: 3
Starting system log daemon: syslogd klogd.
Starting NFS common utilities: statd lockd.
Starting internet superserver: inetd.
Starting MontaVista target tools daemon: mvltdmvltd version 2.1 MontaVista Software,Inc.
.
MontaVista(R) Linux(R) Professional Edition 4.0 (0501140)
192.168.1.197 login:
你的这个问题我查一下,类似的情况还是有的。硬件不知是否你们自己做的呢?如果你们确定硬件没有问题,请点击以下链接更新一下PSP,一般是内核驱动的BUG:
software-dl.ti.com/.../index.html
我们不进行电话支持的,流程很麻烦。。。抱歉。
你的信息显示“version 2.6.10_mvl401-davinci_evm (root@localhost.localdomain) (gcc versio n 3.4.3 (MontaVista 3.4.3-25.0.30”你的Linux版本是2.6.10的,MontaVista 3.4.3的,都是很低的版本。
而'LSP 2.00' Production Release的版本是Linux Support Package (Kernel 2.6.18),MontaVista Pro 5.0.0。
另外你的板子如果不是TI的EVM板,这个问题我不能给你保证。
1. 硬件是否是公板
2. 鼠标是USB1.1的吧,是直接接的开发板的USB Host么
3. 是每次都稳定的出Error还是随机出现
我猜应该不是公板,是DM6446的VBUS那块硬件电路和内核的驱动不匹配造成的
现在1.1的usb鼠标比较少吧?我们使用的是联想台式机的鼠标。
只能说经常出现VBUS_ERR的错误,很少能成功使用usb鼠标。
不是公板。那如何解决?能详细点吗?
usb 1-1: new low speed USB device using musb_hdrc and address 2
input: USB HID v1.11 Mouse [USB Optical Mouse] on usb-musb_hdrc-1
这是正常启动后的打印出来的usb部分信息,这是说我的鼠标是1.1,还是板子的usb是1.1 ?
我看usb的文档,板子上应该是2.0的usb。
如果我使用usb1.1鼠标在usb2.0上,会是产生这个问题的原因吗? 我更换一下可行吗?
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
。。。。。。。。。。。。。。。。。。。
usb 1-1: new low speed USB device using musb_hdrc and address 2
input: USB HID v1.11 Mouse [USB Optical Mouse] on usb-musb_hdrc-1
这些信息说明什么?我该使用什么样的usb鼠标?