This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: LCD配置相关问题

Part Number: AM3352

您好,使用fbdev driver。

对于LCD寄存器中DMA地址如何配置,DMA0和1最后获得的地址是一样的吗?这样做的意义是什么?还是说DMA0从DDR获取数据时,DMA1对外输出输出,然后在lcdc_irq_handler_rev02中切换DMA1和0,DMA1从DDR获取数据,DMA0对外输出,这样的理解是否正确?

另外,配合QT做显示,但偶发的会出现短暂黑屏1s,马上又会恢复,或者有时会有1分钟的黑屏,但是器件语音正常,说明应用程序工作正常,这种可能会是什么原因呢?

谢谢!