Device:C6678 Device Functional Simulator, big endian
假设现在程序运行在core2上,在config时只选择TMS320C66X_2,如下图
选择TMS320C66X_2,如下图
run to symbol:
这样配置,运行起来之后,进不了main()函数,请问一下,还有什么需要的配置吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Device:C6678 Device Functional Simulator, big endian
假设现在程序运行在core2上,在config时只选择TMS320C66X_2,如下图
选择TMS320C66X_2,如下图
run to symbol:
这样配置,运行起来之后,进不了main()函数,请问一下,还有什么需要的配置吗?
我也遇到同样问题了,有答案了吗,麻烦教授:37804037@qq.com
恩,好的。现在有很小的概率可以进main(), 但是按一下F6就卡死了。如果下断点,用F8执行,还是可以跑到断点,但是很卡,不是很清楚是什么原因。
问题解决了,问题是设置的L2 cache的大小。
C6678 L2 cache最大512K,但是设置512K似乎有问题,具体是什么原因导致的不清楚。
设置成256K,一切OK。