This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3894启动问题



各位大师,想请教一下。

我们现在正准备小批一个产品,但临时发现使用的MCU  AM3894经常会出现启动不了的现象,我们使用的电源管理芯片是TPS659110。我在测试中发现,出现启动不了主要在以下几种情况中容易出现:

1、多次连续启动中,很容易出现启动不了;
2、如果在启动时,使用USB转串口的连接器把AM3894的串口2(AM3894的M1、L2脚)与电脑的USB连接,则容易出现启动不了;
3、机子在不通电一段长时间后,首次启动比较容易出现启动不了;
4、如果长时间通电,AM3894在比较热的情况下,如果重启容易出现启动不了。
 
以下附件是我测试的TPS659110各个电压的上电时序,请帮忙查看是否正常,在AM3894的开发板原理图中,各个电压的上电间隔都是10MS级的,但是我们量到的间隔大部分是2MS,而这个间隔我们没有用程序修改过,是出厂默认值。
另外的PDF文件是TPS659110的原理图。
picture.zip