TRM 4129页有这样一句话:
If MMC1 is used the GPMC interface is not usable, due to pin muxing options.
请确认这是否意味着如果用eMMC,除非直接接到MMC0上,否则是无法使用需要GPMC接口的Quicklogic的摄像头芯片的?
谢谢。
matianfu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,Gary,我就是想eMMC和quicklogic的camif一起用。我现在的理解是这样:
1. TI的手册上只建议用MMC0接SD卡座,MMC1接eMMC/eSD。TRM 26.1.7.5.2
2. MMC1占用了GPMC的Addr/Data复用界面,如果用了MMC1就不能用GPMC的quicklogic的camif了。
似乎我只有两个选择:
1. 不用eMMC,用NAND。NAND和QL/CAMIF共用GPMC界面,感觉这样不太好,因为预览或者摄像的时候,后台有程序访问文件系统,会有影响。不知道是否有TI客户这样做过,效果如何?
2. 用eMMC,但是没办法用eMMC boot;GPMC给QL/CAMIF,这个导致MMC1最多只能接4bit界面,那么eMMC只好接到MMC2上去,可以8bit,MMC1接wifi了。然后系统内部的memory boot只有用spi flash或者nand了,放boot loader,文件系统还是在eMMC(MMC2)上。这个貌似可以保证camif的带宽。
上述方案可行么?请给些建议,谢谢。
matianfu