通过DSP6713的EMIF接口和FPGA进行通信,在FPGA内写了一个双口RAM,同步输入,异步输出。下面的截图是用在线逻辑分析仪chipscope捕获的DSP的EMIF接口的数据,DSP内的代码实现的操作时从地址0一直进行写操作,直到地址7,相应地址的数据分别是1~8,为什么在DSP通过EMIF写的时候 地址线上会有其他的地址出现,比如地址4和地址5中间的0和2,为什么在地址4之后应该是5,而实际上是先从4变为0然后变为2再变成地址5,并且,在写操作的时候数据线上也会出现这种情况,双口RAM的输出数据线上也会出现这种情况,这是什么原因造成的?谢谢!