请问
1、DM6467的VLYNQ接口可以和Altera的FPGA进行通信吗?
2、在Altera里面实现VLYNQ协议是否难度比较大?
3、有没有VLYNQ通信协议可以提供?
4、VLYNQ是否只能和Xinlinx的FPGA通信?
十分感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问
1、DM6467的VLYNQ接口可以和Altera的FPGA进行通信吗?
2、在Altera里面实现VLYNQ协议是否难度比较大?
3、有没有VLYNQ通信协议可以提供?
4、VLYNQ是否只能和Xinlinx的FPGA通信?
十分感谢。
你跑操作系统吗,不跑的话,emif通信最合适。
1. FPGA这边来适应时序,理论上都可以的
2. 难度因人而异
3. 手册上很详细。 此外,还有这个文档http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=spruer8
4. 回答和1一样。只是Xilinx做了IP core而已。时序逻辑都是人写出来的
我想你还是要结合文档具体评估一下用哪个
此外提供一个e2e上的链接供参考,这个问题以前也有人问过,建议常去e2e搜一下,那边的问题库已经很全了。
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/t/31962.aspx
BR,
Eason