各位开发者:
大家好。我用的DSP开发板为TMDXLCDK6748,仿真器为SSD-XDS 510 PLUS,使用仿真器连接开发板时,没有错误,另外一个在外地的同事使用相同型号的开发板和仿真器连接时,报出了Error connecting to the target: (Error -1265 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver. (Emulation package 5.0.569.0)的错误。都用的CCS v5,我把我的target configuration配置文件发给他,结果还是报相同的错误,请教一下,这个错误产生的原因是什么?