This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Keystone-2资料共享][更新]如何在TCI6638 EVM上烧写及运行U-boot和Linux Kernel

大家好,

我们已经推出相关的DSP+ARM SoC及对应的EVM:http://www.advantech.com/Support/TI-EVM/default.aspx

附件是关于如何在搭建相关的Linux环境,并在TCI6638 EVM上烧写运行U-boot及Linux kernel的指南,请参考。

Build and Run U-boot and Linux Kernel on TCI6638 EVM.pdf
  • 大家好:

     

    根据论坛里面的用户反馈,我们更新了一下在TCI6638K2K EVM上面编译,烧写和运行U-Boot及Linux Kernel的操作指南,主要更新如下:

     

    1)新增了UBI file system启动模式的操作说明,包括如何烧写UBI Image以及划分和挂载MTD的UBI分区

    2)新增了修改,更新UBI Image以及应用新UBI Image的操作过程

    3)根据用户反馈,更新了一些表述模糊以及启程关系不清的操作及描述

    注:目前该文档只包含XTCIEVMK2X Rev1.0的相关BMC操作指令,如果用户使用Rev1.1及2.0版本的EVM,BMC相关操作指令会有所不同,会在后续文档中予以更新。