This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM368的启动



大家好,有一个关于DM368启动的问题,想请教一下大家。

首先:BOOTSEL[2:0]决定了启动模式:

            如果BOOTSEL[2:0] ==001 则从AEMIF启动,

            如果BOOTSEL[2:0] !=001则从内部ROM启动RBL,再从其它如nand,SPI,SD,URAT等接口读UBL,再启动。

那么,如果有写了一个不带操作系统的裸机程序xx.bin ,如果不采用AMIF启动方式可以么?比如从SPI启动,可以吗,RBL已经运行,再运行.bin文件,是否可行,谢期待达人们的回复,谢谢了。