This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

画DM365时遇到的问题



我在画DM365的板子。有几个问题想请教一下

(1)在板子的电源部分,我不打算用Ti推荐的专门针对DM365的电源芯片,而是用三个TPS73001芯片,分别输出1.8V,  1.35V和3.3V。

因为DM365起动对电源的起动次序有要求,所有我特意在这三个TPS73001的使能脚EN加延时电路(电阻和电容组成),使它们的起动次序满足要求。

这种方法可以吗?

(2)在DM365手册中,推荐LAYOUT时,层叠的次序是:(信号层1、地层、电源层、信号层2、地层、信号层3)。

我想问,把层叠的次序改为:(信号层1、地层、信号层2、信号层3、电源层、信号层4)。

而且我打算将DDR2的信号走线安排信号层1、信号层2、信号层3。而信号层2、信号层3的距离大于2倍的线宽。

这样 的安排可以吗?

如果不行,问题在哪里?

谢