This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大侠:
我在自己设计的板子上采用SRIO 的 direct IO 方式对FPGA和DSP进行数据传输,FPGA按照一行320*8bits的数据进行读写操作,读写操作241次,DSP作为从端配置模式为0,lx,物理端口采用的是Port0直连,参考输入时钟配置为125M,通信速率1.25G。
目前问题是,板子上电后FPGA与DSP之间可以正常通信,但一段时间后(具体时间不定,可能2分钟,可能20分钟),FPGA与DSP之间的数据通信就失败了,此时DSP查看到Port0_ERR_STAT寄存器的值为0x00030306或者是03030306。
请问引起该种情况的原因是什么呢,如何测试?
非常感谢!