1.最近在看USBSTK5515开发板的例程,有一点不明白,我看到例程中的初始化程序仅仅是对外设时钟选通配置寄存器PCGCR进行了配置,对于CPU映射寄存器没有配置,请问在程序运行的时候这些寄存器是采用默认值吗?
2.我想看一下DSP的引导程序,请问应该看什么资料呢?
3.我需要将程序下载到目标板上,然后当接上USB供电的时候,开发板立刻运行程序,能做到吗?该怎么做呢?
问了这么多问题,麻烦大家了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.最近在看USBSTK5515开发板的例程,有一点不明白,我看到例程中的初始化程序仅仅是对外设时钟选通配置寄存器PCGCR进行了配置,对于CPU映射寄存器没有配置,请问在程序运行的时候这些寄存器是采用默认值吗?
2.我想看一下DSP的引导程序,请问应该看什么资料呢?
3.我需要将程序下载到目标板上,然后当接上USB供电的时候,开发板立刻运行程序,能做到吗?该怎么做呢?
问了这么多问题,麻烦大家了!
你好,
1. memory mapped 寄存器是默认的, 不过在boot之前, bootloader支持对外设寄存器(peripheral register)进行配置.
2. 可以看下面的bootloader文档.
http://www.ti.com/lit/an/sprabd7a/sprabd7a.pdf
3. 可以. DSP reset后, 先是从ROM开始执行bootloader程序.