This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 tftp 加载uImage 出错



你好!

我通过网络加载DM8168 EVM ,u-boot已写入NAND FLASH,

但是tftp时,总是出现Retry count exceeded,

查看了下uImage 大小,2.3M,应该不会超出?

-----

Net:   Detected MACID:90:d7:eb:96:46:6a

Ethernet PHY: GENERIC @ 0x01

DaVinci EMAC

Hit any key to stop autoboot:  0

TI8168_EVM#boot

BOOTP broadcast 1

*** Unhandled DHCP Option in OFFER/ACK: 52

*** Unhandled DHCP Option in OFFER/ACK: 52

DHCP client bound to address 192.168.2.114

Using DaVinci EMAC device

TFTP from server 192.168.2.15; our IP address is 192.168.2.114

Filename 'uImage'.

Load address: 0x81000000

Loading: T T T T T T T T T T T T T T T T T T T T

Retry count exceeded; starting again