hi,
my sdk is DVRRDK3.0. when i set DDR=2G, i use "make -s" to make dvr_rdk, but it will make mistake on board.
erro info bellow:
root@dm816x:/home/libin/2g/ti816x# ./init.sh
*** Bootargs Validated for mem param ***
*** Bootargs Validated for notifyk.vpssm3 params ***
Kernel bootargs validated
numid=1,iface=MIXER,name='PCM Playback Volume'
; type=INTEGER,access=rw---R--,values=2,min=0,max=127,step=0
: values=127,127
| dBscale-min=-63.50dB,step=0.50dB,mute=0
[c6xdsp ] Remote Debug Shared Memory @ 0xbf000000
[m3video] Remote Debug Shared Memory @ 0xbf005020
[m3vpss ] Remote Debug Shared Memory @ 0xbf00a040
Setting DMM priority for [DUCATI ] to [0] ( 0x4e000624 = 0x08000000 )
Setting DMM priority for [HDVICP0 ] to [2] ( 0x4e000634 = 0x0000000a )
Setting DMM priority for [HDVICP1 ] to [2] ( 0x4e000634 = 0x000a0000 )
Setting DMM priority for [HDVICP2 ] to [2] ( 0x4e000634 = 0x00a00000 )
/home/libin/2g/ti816x
root@dm816x:/home/libin/2g/ti816x#
root@dm816x:/home/libin/2g/ti816x# ./load.sh
Attached to slave procId 2.
Loaded file ../firmware/dvr_rdk_fw_m3vpss.xem3 on slave procId 2.
Started slave procId 2.
[m3vpss ] ***** SYSTEM : Frequency <ORG> - 250000000, <NEW> - 280000000
[m3vpss ] notify_attach rtnVal 0
[m3vpss ] initProxyServer rtnVal 0
[m3vpss ]
[m3vpss ] *** UTILS: CPU KHz = 560000 Khz ***
[m3vpss ]
[m3vpss ] 67: SYSTEM : System Common Init in progress !!!
[m3vpss ] 68: SYSTEM: IPC init in progress !!!
[m3vpss ] 68: SYSTEM: Attaching to [HOST] ...
Error in Ipc_control Ipc_CONTROLCMD_LOADCALLBACK [0xffffffff]
Attached to slave procId 1.
Loaded file ../firmware/dvr_rdk_fw_m3video.xem3 on slave procId 1.
Started slave procId 1.
[m3video] ***** SYSTEM : Frequency <ORG> - 250000000, <NEW> - 280000000
and you can see more info on serial port
thank you !