在自己做的开发板上,除了时钟部分是由AD9516产生的100MHz的LVPECL标准的时钟,其余硬件设计基本和EVM6678一样
下载程序时,在Target Configuration文件中给核配置了evmc6678l.gel文件。Debug过程中出现中断,显示了如下的提示信息:
C66xx_0: GEL Output: Setup_Memory_Map...
C66xx_0: GEL Output: Setup_Memory_Map... Done.
C66xx_0: GEL Output:
Connecting Target...
C66xx_0: GEL Output: DSP core #0
C66xx_0: GEL Output: C6678L GEL file Ver is 2.002
C66xx_0: GEL Output: Global Default Setup...
C66xx_0: GEL Output: Setup Cache...
C66xx_0: GEL Output: L1P = 32K
C66xx_0: GEL Output: L1D = 32K
C66xx_0: GEL Output: L2 = ALL SRAM
C66xx_0: GEL Output: Setup Cache... Done.
C66xx_0: GEL Output: Main PLL (PLL1) Setup ...
C66xx_0: GEL Output: PLL in Bypass ...
C66xx_0: GEL Output: PLL1 Setup for DSP @ 1000.0 MHz.
C66xx_0: GEL Output: SYSCLK2 = 333.3333 MHz, SYSCLK5 = 200.0 MHz.
C66xx_0: GEL Output: SYSCLK8 = 15.625 MHz.
C66xx_0: GEL Output: PLL1 Setup... Done.
C66xx_0: GEL Output: DSP core #64 cannot set PSC.
C66xx_0: GEL Output: PA PLL (PLL3) Setup ...
C66xx_0: GEL Output: DSP core #64 cannot set PA PLL
C66xx_0: GEL Output: DDR3 PLL (PLL2) Setup ...
C66xx_0: GEL Output: DSP core #64 cannot set DDR3 PLL
C66xx_0: GEL Output: DDR begin (1333 auto)
C66xx_0: GEL Output: XMC Setup ... Done
C66xx_0: GEL Output:
DDR3 initialization is complete.
C66xx_0: GEL Output: DDR done
C66xx_0: GEL Output: DDR3 memory test... Started
C66xx_0: GEL Output: DDR3 memory test... Failed
C66xx_0: GEL Output: Main PLL (PLL1) Setup ...
C66xx_0: GEL Output: DSP core #64 cannot set PLL1.
C66xx_0: GEL Output: Error in Setting up main PLL, please power cycle the board and re-run Global Default Setup...
请问这可能是什么原因造成的?