This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6455 Debug



大牛们:

             1)对于多核C6678的Launch EVM6678.CCXML文件时,不需要仿真器和目标板的上电连接也能够进入到Debug窗口模式下。但是个人对C6455配置的CCXML文件进行Launch时,是不是必须使用仿真器将PC和目标板进行上电才能进入到Debug模式下?现在我的仿真器Seed XDS560plus有许多问题不能连接,这也就使得不能进入CCS的Debug模式,请问能不能通过修改配置CCXML的信息来实现像EVM6678.CCXML 文件那样脱机(脱离仿真器和目标板)就可以进入到Debug模式呢?因为只有这样才能够进一步考虑进行connect target操作等等。

             2)在配置CCXML文件时,选定芯片设备后,在Emulator_0中有port number :0X0,0x1,0x2,0x3等选项,这些指的是什么?另外在单块电路板上我们发了四块C6455的片子,但是仿真接口(14 pins)只有一个,使用仿真器能够同时对这四个DSP进行仿真操作吗?如果可以需要些甚么样的配置?是不是要在放弃起下放四个C6455芯片设备呢,还要选定Slave processor吗? Please answer detailed! Thanks!