This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

合众达XD560与DSP连接问题 错误代码0x80000200/-291



重启目标板与仿真器多次 都是出现这个错误 开发环境为CCS3.3  在CCS5.1环境下点调试后 无限等待 求解 目标板是自研的 根据成型板子开发的 设计应该没问题。

  • 你好,完整的报错信息是什么?先确定仿真器驱动没问题(可以交叉试验一下别的板子),然后再连接板子。

  • 以下是完整错误信息:

    Error connecting to the target:
    Error 0x80000200/-291
    Fatal Error during: OCS,
    This error was generated by TI's USCIF driver.

    SC_ERR_TST_MEASURE <-291>
    The built-in scan-path length measurement has failed. This indicates
    that the JTAG controller cannot reliably communicate with
    the target DSP's and micro-controllers at that frequency.
    Try specifying the scan-path lengths in the board configuration
    file because the built-in scan-path reliability tests cannot be
    performed without knowledge of the scan-path length.


    Sequence ID: 0
    Error Code: -291
    Error Class: 0x80000200

    Board Name: C671x XDS560 Emulator
    Cpu Name: TMS320C6710_0

    Abort:  Close Code Composer Studio.
    Retry:  Try to connect to the target again.
    Cancel:  Remain disconnected from the target
    Diagnostic: Run diagnostic utility.

    别的板子连接没有问题

  • 在targetconfiguration窗口下,选择仿真器驱动等完成后,先不要点debug,而是点击Test connection,能测试通过吗?

  • 在CCS3.3下连接不通过 出现刚才那个错误代码的问题

  • 如果其他板子都可以通过这个仿真器正常连接,说明仿真器问题应该不大。请先检查检查DSP供电是否正常;检查晶振是否起振,DSP上电正常情况下,查看CLKOUT 引脚,会有脉冲输出。就是说,先检查DSP是否可以正常启动,如果可以再详细检查JTAG接口电路是否有问题。

  • 你好,请问你的问题解决了么?我遇到类似的问题,以前生产的几套板卡都是没有问题,最近刚生产的仿真器连接不上,并且拿好的老板卡也连不上了。