This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678的SPI通信配置完成后,发送数据,示波器观察不到没有任何信号

先按照PDK的例子进行初始化spi_claim,然后用spi_xfer持续发送数据,但是用示波器观察CLK,CS0,CS1,MISO,MOSI都没有任何波形。

函数原型如下,采用的FPGA的CS

spi_claim
(
uint32_t cs,
uint32_t freq
)
{
uint32_t scalar;

// PLIBSPILOCK() //wy

/* Enable the SPI hardware */
SPI_SPIGCR0 = CSL_SPI_SPIGCR0_RESET_IN_RESET;
spi_delay (2000);
SPI_SPIGCR0 = CSL_SPI_SPIGCR0_RESET_OUT_OF_RESET;

/* Set master mode, powered up and not activated */
SPI_SPIGCR1 = (CSL_SPI_SPIGCR1_MASTER_MASTER << CSL_SPI_SPIGCR1_MASTER_SHIFT) |
(CSL_SPI_SPIGCR1_CLKMOD_INTERNAL << CSL_SPI_SPIGCR1_CLKMOD_SHIFT);


/* CS0, CS1, CLK, Slave in and Slave out are functional pins */
if (cs == 0)
{
SPI_SPIPC0 = (CSL_SPI_SPIPC0_SCS0FUN0_SPI << CSL_SPI_SPIPC0_SCS0FUN0_SHIFT) |
(CSL_SPI_SPIPC0_CLKFUN_SPI << CSL_SPI_SPIPC0_CLKFUN_SHIFT) |
(CSL_SPI_SPIPC0_SIMOFUN_SPI << CSL_SPI_SPIPC0_SIMOFUN_SHIFT) |
(CSL_SPI_SPIPC0_SOMIFUN_SPI << CSL_SPI_SPIPC0_SOMIFUN_SHIFT);
}
else if (cs == 1)
{
SPI_SPIPC0 = ((CSL_SPI_SPIPC0_SCS0FUN1_SPI << CSL_SPI_SPIPC0_SCS0FUN1_SHIFT) |
(CSL_SPI_SPIPC0_CLKFUN_SPI << CSL_SPI_SPIPC0_CLKFUN_SHIFT) |
(CSL_SPI_SPIPC0_SIMOFUN_SPI << CSL_SPI_SPIPC0_SIMOFUN_SHIFT) |
(CSL_SPI_SPIPC0_SOMIFUN_SPI << CSL_SPI_SPIPC0_SOMIFUN_SHIFT)) & 0xFFFF;
}

/* setup format */
scalar = ((SPI_MODULE_CLK / freq) - 1 ) & 0xFF;

if ( cs == 0)
{
SPI_SPIFMT0 = (8 << CSL_SPI_SPIFMT_CHARLEN_SHIFT) |
(scalar << CSL_SPI_SPIFMT_PRESCALE_SHIFT) |
(CSL_SPI_SPIFMT_PHASE_DELAY << CSL_SPI_SPIFMT_PHASE_SHIFT) |
(CSL_SPI_SPIFMT_POLARITY_LOW << CSL_SPI_SPIFMT_POLARITY_SHIFT) |
(CSL_SPI_SPIFMT_SHIFTDIR_MSB << CSL_SPI_SPIFMT_SHIFTDIR_SHIFT);
}
else if ( cs == 1)
{
SPI_SPIFMT0 = (16 << CSL_SPI_SPIFMT_CHARLEN_SHIFT) |
(scalar << CSL_SPI_SPIFMT_PRESCALE_SHIFT) |
(CSL_SPI_SPIFMT_PHASE_NO_DELAY << CSL_SPI_SPIFMT_PHASE_SHIFT) |
(CSL_SPI_SPIFMT_POLARITY_LOW << CSL_SPI_SPIFMT_POLARITY_SHIFT) |
(CSL_SPI_SPIFMT_SHIFTDIR_MSB << CSL_SPI_SPIFMT_SHIFTDIR_SHIFT);
}

/* hold cs active at end of transfer until explicitly de-asserted */
data1_reg_val = (CSL_SPI_SPIDAT1_CSHOLD_ENABLE << CSL_SPI_SPIDAT1_CSHOLD_SHIFT) |
(0x02 << CSL_SPI_SPIDAT1_CSNR_SHIFT);
if (cs == 0)
{
SPI_SPIDAT1 = (CSL_SPI_SPIDAT1_CSHOLD_ENABLE << CSL_SPI_SPIDAT1_CSHOLD_SHIFT) |
(0x02 << CSL_SPI_SPIDAT1_CSNR_SHIFT);
}

/* including a minor delay. No science here. Should be good even with
* no delay
*/
if (cs == 0)
{
SPI_SPIDELAY = (8 << CSL_SPI_SPIDELAY_C2TDELAY_SHIFT) |
(8 << CSL_SPI_SPIDELAY_T2CDELAY_SHIFT);
/* default chip select register */
SPI_SPIDEF = CSL_SPI_SPIDEF_RESETVAL;
}
else if (cs == 1)
{
SPI_SPIDELAY = (6 << CSL_SPI_SPIDELAY_C2TDELAY_SHIFT) |
(3 << CSL_SPI_SPIDELAY_T2CDELAY_SHIFT);
}

/* no interrupts */
SPI_SPIINT0 = CSL_SPI_SPIINT0_RESETVAL;
SPI_SPILVL = CSL_SPI_SPILVL_RESETVAL;

/* enable SPI */
SPI_SPIGCR1 |= ( CSL_SPI_SPIGCR1_ENABLE_ENABLE << CSL_SPI_SPIGCR1_ENABLE_SHIFT );

// if (cs == 1)
// {
// SPI_SPIDAT0 = 1 << 15;
// spi_delay (10000);

/* Read SPIFLG, wait untill the RX full interrupt */
//wy
// if ( (SPI_SPIFLG & (CSL_SPI_SPIFLG_RXINTFLG_FULL<<CSL_SPI_SPIFLG_RXINTFLG_SHIFT)) )
// {
/* Read one byte data */
// scalar = SPI_SPIBUF & 0xFF;
/* Clear the Data */
// SPI_SPIBUF = 0;
// }
// else
// {
/* Read one byte data */
// scalar = SPI_SPIBUF & 0xFF;
// return SPI_EFAIL;
// }
// }

return SPI_EOK;
}

spi_xfer
(
uint32_t nbytes,
uint8_t* data_out,
uint8_t* data_in,
Bool terminate
)
{
uint32_t i, buf_reg;
uint8_t* tx_ptr = data_out;
uint8_t* rx_ptr = data_in;


/* Clear out any pending read data */
SPI_SPIBUF;

for (i = 0; i < nbytes; i++)
{
/* Wait untill TX buffer is not full */
while( SPI_SPIBUF & CSL_SPI_SPIBUF_TXFULL_MASK );

/* Set the TX data to SPIDAT1 */
data1_reg_val &= ~0xFFFF;
if(tx_ptr)
{
data1_reg_val |= *tx_ptr & 0xFF;
tx_ptr++;
}

/* Write to SPIDAT1 */
if((i == (nbytes -1)) && (terminate))
{
/* Release the CS at the end of the transfer when terminate flag is TRUE */
SPI_SPIDAT1 = data1_reg_val & ~(CSL_SPI_SPIDAT1_CSHOLD_ENABLE << CSL_SPI_SPIDAT1_CSHOLD_SHIFT);
} else
{
SPI_SPIDAT1 = data1_reg_val;
}

/*
// Read SPIBUF, wait untill the RX buffer is not empty
while ( SPI_SPIBUF & ( CSL_SPI_SPIBUF_RXEMPTY_MASK ) );

// Read one byte data
buf_reg = SPI_SPIBUF;
if(rx_ptr)
{
*rx_ptr = buf_reg & 0xFF;
rx_ptr++;
}
*/
}

return SPI_EOK;

}

调用函数的代码如下:

Uint32 ret;
uint8_t idcode[3]; /* Initialize the SPI interface */
idcode[0]=0x12;
idcode[1]=0x23;
idcode[2]=0x34;
idcode[3]=0x45;

/* Claim the SPI controller */
spi_claim(SPI_FPGA_CS, SPI_MAX_FREQ/2);

/* Read the ID codes */

int a;
a=0;
while(1)
{
a++;
spi_xfer(4,idcode,idcode,1);
}


spi_release();

在板子上观察不到任何波形,请教问题出在那里?谢谢