采用TVP5158在DM6467上做的视频采集,经过264编码以后,采用视频播放软件进行播放,发现,在动态图像时,视频中的边缘有锯齿现象。比如图像中有1本书,如果图像在移动,则书的边缘就会有锯齿现象。请问这是什么原因呢?
PS:TVP5158配置是参照之士提供的代码。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这位大牛你好!
我最近刚入手视频处理,我们有个需要,用DM6467+TVP5158做两路D1视频编码,我们采用的是之士提供的源码,也就是mcvp_tvp5158,我按照行交错模式配置5158,按照例子代码提取两个通道的数据,分别存放到两个buf里面,然后去H264编码,封装成TS,最终没有图像出现。后来我将分离出来的每个通道的原始数据保存,用YUVplayer播放,全是花屏,没有看到图像。我就怀疑是我提取每个通道原始数据的代码出现问题,我将mcvp_tvp5158的每个通道数据保存,也是一样的没有有效视频,mcvp_tvp5158是能正常运行的,它没有压缩,只是通过DaVinci_dsiplay直接显示出来的,我现在很困惑,我也将422转成420,但是还没有用,能给我提点建议吗?求指导!万分感谢!
运动物体的横纹还是de-interlace算法策略的问题,和5158关系不大。 你可以把内存里的奇偶场单独导出来,手工合一下看看这个锯齿还在不在。
这个能帮忙提供点提示吗?谢谢您!我们是6467t+TVP5158,不知道您说的这个de-interlace感觉是在mcvip里面,这个跟264的编码器格式参数有关系吗?谢谢!