您好:
我用定时器8产生EDMA3控制器0输入事件,让EDMA3去进行数据传输,传输完成产生DMA中断.我发现,我在CORE0上运行时,DMA没有进行数据传输,但是我在core1-core7上运行同样的工程时,DMA数据传输正常.请问,这有可能是什么原因造成的?误操作某些寄存器会导致这种情况吗? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Andy Yin ,您好:
8个核我使用的是同一个.out文件,我将out文件加载到core0运行时,DMA没有传输数据,然后系统复位,加载到core1,运行正常,core2-core7的操作同core1都正常,DMA使用的地址均是全局地址,让我奇怪的时,8个核硬件上结构都一样,我使用相同的out文件,在不同核上运行,还有不同的效果,费解! 需要说明的是,我之前直接操作寄存器配置DMA传输数据时,偶偶也出现这种情况,我现在是用csl库实现的,之前和现在,我都是手动触发DMA事件,进行DMA传输, 然而,我现在将DMA触发事件改成定时器触发,core0运行就很正常!