Other Parts Discussed in Thread: TMS320C6748
你好,我用得是TMS320C6748 DSP Development KIT, 用CCS5.4编程。用得是TI给的例子,也就是在C6748_StarterWare_1_20_03_03文件里的demoLedIf。
程序如下:
#include "gpio.h"
#include "soc_C6748.h"
#include "hw_psc_C6748.h"
#include "lcdkC6748.h"
#include "demoCfg.h"
static unsigned int ledState = 0;
void LedIfConfig(void)
{GPIOBank6Pin12PinMuxSetup();
GPIODirModeSet(SOC_GPIO_0_REGS, 109, GPIO_DIR_OUTPUT);}
void LedToggle(void)
{
if(ledState == 0) ledState = 1;
else ledState = 0;
GPIOPinWrite(SOC_GPIO_0_REGS, 109, ledState); }
void LedOff(void)
{ GPIOPinWrite(SOC_GPIO_0_REGS, 109, GPIO_PIN_HIGH); }
编译的时候就会出现
#10010 errors encountered during linking; "LED.out" not built 和 #10234-D unresolved symbols remain
**** Build of configuration Debug for project LED ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 'Building file: ../main.c' 'Invoking: C6000 Compiler' "C:/ti/ccsv5/tools/compiler/c6000_7.4.2/bin/cl6x" -mv6740 --abi=coffabi -g --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.2/include" --define=c6748 --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp" "../main.c" 'Finished building: ../main.c' ' ' 'Building target: LED.out' 'Invoking: C6000 Linker' "C:/ti/ccsv5/tools/compiler/c6000_7.4.2/bin/cl6x" -mv6740 --abi=coffabi -g --define=c6748 --display_error_number --diag_warning=225 --diag_wrap=off -z --stack_size=0x800 -m"LED.map" --heap_size=0x800 -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.2/lib" -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.2/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="LED_linkInfo.xml" --rom_model -o "LED.out" "./main.obj" -l"libc.a" "../C6748.cmd" <Linking>
undefined first referenced symbol in file --------- ---------------- _main C:\ti\ccsv5\tools\compiler\c6000_7.4.2\lib\rts6740.lib<args_main.obj>
error #10234-D: unresolved symbols remain >> Compilation failure error #10010: errors encountered during linking; "LED.out" not built gmake: *** [LED.out] Error 1 gmake: Target `all' not remade because of errors.
**** Build Finished ****
请问这是什么问题呢?谢谢