This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 vpif interface problem



Hello,

   I got a problem when using the vpif interface of DM6467.

 When I read the user guide of vpif 

I think it means that when I configure this bit of CH0_CTRL register as 0, the input data should be changed at the rising edge of the input clock,and , in turn , the vpif interface will capture the data at the falling edge of th input clock. And the vice versa.

But the fact is just in the opposite side.

When I control the input data  being changed at the rising edge of the input clock, and configure this bit of CH0_CTRL register as 0, sometimes the vpif interface cannot receive video data properly.

If I control the input data  being changed at the rising edge of the input clock, and configure this bit of CH0_CTRL register as 1,  the vpif interface will receive video data properly all the time.

So I wonder if there's something wrong with the vpif datasheet or if I have a misunderstanding of it.

Is there anybody can help me ? Thank you very much!

  • 你好,

    我认为这需要从输入,或者输出的角度来看。

    如果是输入口,时钟上升沿有效,那就需要输出的数据在下降沿输出,这样做时钟的上升沿就可以正确采集到数据。

    如果是输出口,时钟上升沿有效,据需要在上升沿发出数据,而接收端需要在时钟的下降沿接受数据。

  • vpif 接口的channel0就是输入口。我现在不理解,配置与时钟的关系。我们都知道,如果数据在时钟上升沿变化,那么我们在下降沿采集才不会出错。比如,我们是通过FPGA向VPIF接口送数据的,配置成0时,FPGA端输入数据应该是在时钟上升沿变化还是下降沿变化?