您们好,我是一个学生,想请问下,如果想做一个ARM9和FPGA通过SPI接口通信的一个项目,现在想选择一个ARM9芯片,请问下最好是选择什么类型的,主要是基于以下几方面的考虑,最好是内带FLASH和SRAM的,这样可以不用外扩,方便以后做板,现在只是实验而已,还有能接5寸左右的液晶彩屏,之前是DSP和FPGA的通信,现在想改成ARM9和FPGA的通信,之前DSP的代码有400K左右,如果上了LINUX操作系统,片内自己带的FLASH和SRAM还够吗?麻烦了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您们好,我是一个学生,想请问下,如果想做一个ARM9和FPGA通过SPI接口通信的一个项目,现在想选择一个ARM9芯片,请问下最好是选择什么类型的,主要是基于以下几方面的考虑,最好是内带FLASH和SRAM的,这样可以不用外扩,方便以后做板,现在只是实验而已,还有能接5寸左右的液晶彩屏,之前是DSP和FPGA的通信,现在想改成ARM9和FPGA的通信,之前DSP的代码有400K左右,如果上了LINUX操作系统,片内自己带的FLASH和SRAM还够吗?麻烦了!