Part Number: TDA4VM-Q1
TDA4的功能引脚,例如DSI的通信引脚(TXP TXN),CSI的通信引脚,serdes的通信引脚,MMC的通信引脚,SPI的通信引脚,CAN的通信引脚,USB的通信引脚,RGMII通信引脚,GPIO不使用时,空端子如何处理
是不是只需要关注6.5 Connections for Unused Pins这里面提到的就可以,其他的都可以悬空处理
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM-Q1
TDA4的功能引脚,例如DSI的通信引脚(TXP TXN),CSI的通信引脚,serdes的通信引脚,MMC的通信引脚,SPI的通信引脚,CAN的通信引脚,USB的通信引脚,RGMII通信引脚,GPIO不使用时,空端子如何处理
是不是只需要关注6.5 Connections for Unused Pins这里面提到的就可以,其他的都可以悬空处理
是的,Note部分也有说明。
All other unused signal balls without Pad Configuration Register can be left unconnected.
All other unused signal balls with a Pad Configuration Register can be left unconnected with their multiplexing mode set to GPIO input and internal pulldown resistor enabled.
所以就是复用的引脚配置成GPIO,并且使能内部下拉,不是复用的直接悬空处理就好,对吧