AM1808硬件版本号为2.0,用官网给的UART Boot Host.exe 可以通过串口下载u-boot_uart_ais_v1.bin,但是BOOT模式改为DEBUG后用JLINK的时候,载入程序后内部RAM的数据是不对的,不能正常跳转!
开发环境为MDK;
请问:这会是硬件方面设计还有没考虑到的地方?
电源上电顺序,BOOT模块,保留脚(RSVDN、RSV2)、以及其它未用到的引脚都是按手册的要求进行连接,还会有哪方面的因素会导致JLINK载入程序时会使内部RAM出错呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
接NOR肯定是这样了。
不过谁也不会想到在板上接上GB的NOR吧
不是NOR FLASH,而是NAND FLASH,这里每个CS只有32M的地址空间,而代理商给的DEMO板却接了128M的NAND FLASH。。。再次请教,谢谢
终于搞明白了,里面没有FLASH CONTROLER,而是通过地址线、数据线按正一定的时序对NAND FLASH进行读写,所以,32M地址空间跟NAND FLASH里的空间并不是一一对应的,所以,NAND FLASH 不受此限制,相反,NOR FLASH 内部就与32M地址空间一一对应,所以最大只能接32M的NOR FLASH;