Other Parts Discussed in Thread: ADS131A04
我最最近学习使用官方例程MMC_SD_SETUP。
在设置完MMC寄存器后,开始初始化SD卡,流程如下:
但在实际用示波器测试时,CMD0与ACMD41间还多发了一条指令,且ACMD41发送后没能得到SD卡的反馈QwQ。
硬件连接如下,由于我的DSP板子供电不太稳定,因此SD供电是由STM32完成的,STM32与DSP进行了共地。
期待工程师们的解答!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我最最近学习使用官方例程MMC_SD_SETUP。
在设置完MMC寄存器后,开始初始化SD卡,流程如下:
但在实际用示波器测试时,CMD0与ACMD41间还多发了一条指令,且ACMD41发送后没能得到SD卡的反馈QwQ。
硬件连接如下,由于我的DSP板子供电不太稳定,因此SD供电是由STM32完成的,STM32与DSP进行了共地。
期待工程师们的解答!
DSP板子供电不太稳定
最好先解决供电的问题,其他接口都能稳定工作么?还是只有sd接口不能工作?
CSL里的MMC_SD_SETUP例程是在TI开发板上验证过的,如果您板子的硬件和TI开发板一样的话,应该可以运行的,所以建议还是先解决DSP供电不稳定的问题再看。