Part Number: AMIC110
Hi,
We will develop a product that need to implement Muli-Protocol including Profinet, Profisafe,EtherCAT, Ethernet/IP. We want to implement it by PHY chip. Is there solution can meet our needs? Does TI provide protocol stack?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMIC110
Hi,
We will develop a product that need to implement Muli-Protocol including Profinet, Profisafe,EtherCAT, Ethernet/IP. We want to implement it by PHY chip. Is there solution can meet our needs? Does TI provide protocol stack?
We will develop a product that need to implement Muli-Protocol including Profinet, Profisafe,EtherCAT, Ethernet/IP
可以的,请参考:
Does TI provide protocol stack?
请阅读以下文档:
Hello Nancy:
Thank you for your reply!I read the link you provided, which mentioned that the Sitara processor can provide automatic detection of various industrial protocols. If we want to implement our product functions at the same time, do we need to add another MCU? If necessary, then Sitara How to match with MCU.
In addition, our products also need to implement Profisafe. Can this Sitara processor implement Profisafe? How should we implement Profisafe? thanks
If we want to implement our product functions at the same time, do we need to add another MCU? If necessary, then Sitara How to match with MCU.
请问是需要多种协议同时实现吗?
our products also need to implement Profisafe. Can this Sitara processor implement Profisafe?
不支持。
Hi Nancy;
1.我们对同时实现多种协议的需求是:多种协议栈能同时存储在处理器中,当外部接了某个设备时(通信协议未知),处理器可以自动识别到该设备的通信协议类型并与之通信。
2.请问TI有没有可以支持Profisafe的处理器或者方案,谢谢!
Hi Nancy:
我通过查资料得到一些信息:Profisafe可以通过软件的方式实现,但是前提是需要有支持该软件的器件,我想知道TI是否有可以支持Profisafe的器件?谢谢!
我们对同时实现多种协议的需求是:多种协议栈能同时存储在处理器中,当外部接了某个设备时(通信协议未知),处理器可以自动识别到该设备的通信协议类型并与之通信。
我对详细实现细节不太熟悉,以下文档中的实现无法满足您的需求吗?
https://www.ti.com/lit/ug/tidua28a/tidua28a.pdf
:Profisafe可以通过软件的方式实现,但是前提是需要有支持该软件的器件,我想知道TI是否有可以支持Profisafe的器件?谢谢!
我没有搜到相关支持的器件,您可以到英文论坛问问。