Part Number: AM3352
参照网上资料,控制无效:
echo "0" > "/sys/bus/usb/devices/usb1/power/autosuspend_delay_ms"
echo "auto" > "/sys/bus/usb/devices/usb1/power/control"
linux内核版本为: 4.19.59;
求助各位大神...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Processor SDK Linux 06_01_00_08;
日志如下:
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.59-g5f8c1c6121 (root@laifuqi-vm) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03)) #103 PREEMPT Tue Oct 13 16:22:23 CST 2020
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x EVM
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (neon)
[ 0.000000] random: get_random_bytes called from start_kernel+0x7c/0x41c with crng_init=0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/ram rw init=linuxrc
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 449168K/524288K available (9216K kernel code, 331K rwdata, 2904K rodata, 1024K init, 276K bss, 25968K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (10208 kB)
[ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (1024 kB)
[ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 332 kB)
[ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 277 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 25000000 Hz
[ 0.000018] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 85899345900ns
[ 0.000039] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 76450417870 ns
[ 0.000051] OMAP clocksource: timer1 at 25000000 Hz
[ 0.000495] timer_probe: no matching timers found
[ 0.000706] Console: colour dummy device 80x30
[ 0.000769] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
[ 0.089049] pid_max: default: 32768 minimum: 301
[ 0.089282] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089297] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090176] CPU: Testing write buffer coherency: ok
[ 0.091164] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.091326] rcu: Hierarchical SRCU implementation.
[ 0.091716] EFI services will not be available.
[ 0.093219] devtmpfs: initialized
[ 0.101914] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.102343] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.102368] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.106120] pinctrl core: initialized pinctrl subsystem
[ 0.106918] DMI not present or invalid.
[ 0.107320] NET: Registered protocol family 16
[ 0.109912] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.130525] l4_wkup_cm:clk:0010:0: failed to disable
[ 0.171716] cpuidle: using governor ladder
[ 0.171756] cpuidle: using governor menu
[ 0.185653] No ATAGs?
[ 0.185672] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.202952] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.206924] SCSI subsystem initialized
[ 0.207198] usbcore: registered new interface driver usbfs
[ 0.207258] usbcore: registered new interface driver hub
[ 0.207378] usbcore: registered new device driver usb
[ 0.208022] pps_core: LinuxPPS API ver. 1 registered
[ 0.208035] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.208060] PTP clock support registered
[ 0.208084] EDAC MC: Ver: 3.0.0
[ 0.209406] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.210043] Advanced Linux Sound Architecture Driver Initialized.
[ 0.211391] clocksource: Switched to clocksource timer1
[ 0.220726] NET: Registered protocol family 2
[ 0.221705] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes)
[ 0.221743] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.221791] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.221837] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.221949] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.221973] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.222169] NET: Registered protocol family 1
[ 0.222798] RPC: Registered named UNIX socket transport module.
[ 0.222814] RPC: Registered udp transport module.
[ 0.222821] RPC: Registered tcp transport module.
[ 0.222828] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.223977] Trying to unpack rootfs image as initramfs...
[ 0.224749] rootfs image is not initramfs (no cpio magic); looks like an initrd
[ 0.268383] Freeing initrd memory: 6732K
[ 0.268990] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.270568] Initialise system trusted keyrings
[ 0.270915] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.276342] NFS: Registering the id_resolver key type
[ 0.276390] Key type id_resolver registered
[ 0.276399] Key type id_legacy registered
[ 0.276447] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.283224] Key type asymmetric registered
[ 0.283248] Asymmetric key parser 'x509' registered
[ 0.283340] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.283355] io scheduler noop registered
[ 0.283364] io scheduler deadline registered
[ 0.283629] io scheduler cfq registered (default)
[ 0.283642] io scheduler mq-deadline registered
[ 0.283651] io scheduler kyber registered
[ 0.285706] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 0.290318] omap_uart 44e09000.serial: no wakeirq for uart0
[ 0.290544] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a OMAP UART0
[ 0.923850] console [ttyO0] enabled
[ 0.928278] omap_uart 48022000.serial: no wakeirq for uart1
[ 0.934347] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a OMAP UART1
[ 0.944630] omap_uart 481aa000.serial: no wakeirq for uart5
[ 0.950601] 481aa000.serial: ttyO5 at MMIO 0x481aa000 (irq = 35, base_baud = 3000000) is a OMAP UART5
[ 0.962032] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 0.971630] random: fast init done
[ 0.975454] random: crng init done
[ 0.990854] brd: module loaded
[ 1.001778] loop: module loaded
[ 1.006000] SCSI Media Changer driver v0.25
[ 1.010702] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.020184] spidev spi0.0: buggy DT: spidev listed directly in DT
[ 1.026691] ------------[ cut here ]------------
[ 1.031572] WARNING: CPU: 0 PID: 1 at drivers/spi/spidev.c:730 spidev_probe+0x178/0x1b4
[ 1.039951] Modules linked in:
[ 1.043175] CPU: 0 PID: 1 Comm: swapper Not tainted 4.19.59-g5f8c1c6121 #103
[ 1.050552] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 1.056944] Backtrace:
[ 1.059517] [<c010bac4>] (dump_backtrace) from [<c010bd2c>] (show_stack+0x18/0x1c)
[ 1.067461] r6:00000000 r5:c0c3e738 r4:00000000 r3:1235dada
[ 1.073408] [<c010bd14>] (show_stack) from [<c09aa790>] (dump_stack+0x20/0x28)
[ 1.080981] [<c09aa770>] (dump_stack) from [<c0128564>] (__warn+0xf0/0x118)
[ 1.088289] [<c0128474>] (__warn) from [<c01285d8>] (warn_slowpath_null+0x4c/0x54)
[ 1.096231] r8:c0e397f4 r7:c0e8a6f0 r6:000002da r5:c0c3e738 r4:c05be794
[ 1.103265] [<c012858c>] (warn_slowpath_null) from [<c05be794>] (spidev_probe+0x178/0x1b4)
[ 1.111932] r6:c0e397e4 r5:db25ec00 r4:db25ec00
[ 1.116770] [<c05be61c>] (spidev_probe) from [<c05bb4e8>] (spi_drv_probe+0x88/0xa8)
[ 1.124802] r8:c0e397f4 r7:c0e8a6f0 r6:c0e397e4 r5:00000000 r4:db25ec00
[ 1.131837] [<c05bb460>] (spi_drv_probe) from [<c050da18>] (really_probe+0x210/0x2b0)
[ 1.140037] r6:00000000 r5:c0e8a6ec r4:db25ec00 r3:c05bb460
[ 1.145978] [<c050d808>] (really_probe) from [<c050dcb8>] (driver_probe_device+0x64/0x17c)
[ 1.154648] r10:00000000 r9:db25ec00 r8:db25ec00 r7:00000001 r6:c0e397f4 r5:dc061be8
[ 1.162858] r4:c0e397f4 r3:00000000
[ 1.166605] [<c050dc54>] (driver_probe_device) from [<c050df88>] (__device_attach_driver+0x9c/0xb4)
[ 1.176093] r10:00000000 r8:c0e8a6c8 r7:00000001 r6:db25ec00 r5:dc061be8 r4:c0e397f4
[ 1.184317] [<c050deec>] (__device_attach_driver) from [<c050bd4c>] (bus_for_each_drv+0x4c/0x94)
[ 1.193531] r6:c050deec r5:dc061be8 r4:00000000 r3:00000000
[ 1.199461] [<c050bd00>] (bus_for_each_drv) from [<c050dbb0>] (__device_attach+0xa4/0x108)
[ 1.208128] r6:c0e392a0 r5:db25ec34 r4:db25ec00
[ 1.212978] [<c050db0c>] (__device_attach) from [<c050dfb4>] (device_initial_probe+0x14/0x18)
[ 1.221919] r7:db25e800 r6:c0e392a0 r5:db25ec00 r4:db25ec08
[ 1.227850] [<c050dfa0>] (device_initial_probe) from [<c050ccb0>] (bus_probe_device+0x8c/0x94)
[ 1.236886] [<c050cc24>] (bus_probe_device) from [<c050af30>] (device_add+0x3f0/0x5bc)
[ 1.245191] r6:00000000 r5:c0e03048 r4:db25ec08 r3:00000001
[ 1.251120] [<c050ab40>] (device_add) from [<c05bb318>] (spi_add_device+0x90/0x138)
[ 1.259154] r10:dc12c410 r9:00000001 r8:00000000 r7:dc12c410 r6:00000000 r5:db25e800
[ 1.267363] r4:db25ec00
[ 1.270017] [<c05bb288>] (spi_add_device) from [<c05bba3c>] (of_register_spi_device+0x220/0x370)
[ 1.279230] r7:db25e800 r6:00000001 r5:dcb59018 r4:db25ec00
[ 1.285172] [<c05bb81c>] (of_register_spi_device) from [<c05bc0e4>] (spi_register_controller+0x2c4/0x648)
[ 1.295206] r8:db25e800 r7:c0e39324 r6:00000000 r5:dcb59018 r4:db25e800
[ 1.302239] [<c05bbe20>] (spi_register_controller) from [<c05bc4a4>] (devm_spi_register_controller+0x3c/0x78)
[ 1.312638] r10:00000000 r9:db0e8afc r8:db25e800 r7:dc12c410 r6:00000000 r5:db23ba40
[ 1.320834] r4:db25e800
[ 1.323503] [<c05bc468>] (devm_spi_register_controller) from [<c05bff8c>] (omap2_mcspi_probe+0x418/0x4f8)
[ 1.333543] r7:db25eb00 r6:00000000 r5:db25e800 r4:00000000
[ 1.339477] [<c05bfb74>] (omap2_mcspi_probe) from [<c050f7f8>] (platform_drv_probe+0x50/0xa0)
[ 1.348421] r10:00000000 r9:00000000 r8:c0e3984c r7:c0e8a6f0 r6:c0e3984c r5:00000000
[ 1.356631] r4:dc12c410
[ 1.359285] [<c050f7a8>] (platform_drv_probe) from [<c050da18>] (really_probe+0x210/0x2b0)
[ 1.367953] r6:00000000 r5:c0e8a6ec r4:dc12c410 r3:c050f7a8
[ 1.373894] [<c050d808>] (really_probe) from [<c050dcb8>] (driver_probe_device+0x64/0x17c)
[ 1.382564] r10:00000000 r9:c0d3d838 r8:dc12c410 r7:00000000 r6:c0e3984c r5:c0e3984c
[ 1.390761] r4:dc12c410 r3:00000000
[ 1.394518] [<c050dc54>] (driver_probe_device) from [<c050dea8>] (__driver_attach+0xd8/0xdc)
[ 1.403370] r10:00000000 r8:00000000 r7:00000000 r6:dc12c444 r5:c0e3984c r4:dc12c410
[ 1.411585] [<c050ddd0>] (__driver_attach) from [<c050bdf4>] (bus_for_each_dev+0x60/0x84)
[ 1.420149] r6:c050ddd0 r5:c0e3984c r4:dc12c410 r3:00000000
[ 1.426092] [<c050bd94>] (bus_for_each_dev) from [<c050d270>] (driver_attach+0x24/0x28)
[ 1.434486] r6:c0e32778 r5:db23b380 r4:c0e3984c
[ 1.439325] [<c050d24c>] (driver_attach) from [<c050ce90>] (bus_add_driver+0xe8/0x1f4)
[ 1.447632] [<c050cda8>] (bus_add_driver) from [<c050e880>] (driver_register+0x84/0x118)
[ 1.456118] r7:c0d235c0 r6:c0e03048 r5:00000006 r4:c0e3984c
[ 1.462059] [<c050e7fc>] (driver_register) from [<c050f5d8>] (__platform_driver_register+0x48/0x4c)
[ 1.471544] r5:00000006 r4:c0e52f00
[ 1.475297] [<c050f590>] (__platform_driver_register) from [<c0d235d8>] (omap2_mcspi_driver_init+0x18/0x20)
[ 1.485518] [<c0d235c0>] (omap2_mcspi_driver_init) from [<c0102668>] (do_one_initcall+0x50/0x1a0)
[ 1.494834] [<c0102618>] (do_one_initcall) from [<c0d00ea8>] (kernel_init_freeable+0x10c/0x1d0)
[ 1.503960] r10:00000000 r8:c0d3d82c r7:0000011e r6:c0e52f00 r5:00000006 r4:c0d50d1c
[ 1.512184] [<c0d00d9c>] (kernel_init_freeable) from [<c09c1a80>] (kernel_init+0x10/0x124)
[ 1.520842] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c09c1a70
[ 1.529051] r4:00000000
[ 1.531718] [<c09c1a70>] (kernel_init) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 1.539643] Exception stack(0xdc061fb0 to 0xdc061ff8)
[ 1.544947] 1fa0: 00000000 00000000 00000000 00000000
[ 1.553526] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 1.562103] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 1.569027] r4:00000000 r3:ffffffff
[ 1.572790] ---[ end trace 5c70b6188827aeb6 ]---
[ 1.578085] MACsec IEEE 802.1AE
[ 1.581946] libphy: Fixed MDIO Bus: probed
[ 1.587175] e100: Intel(R) PRO/100 Network Driver, 3.5.24-k2-NAPI
[ 1.593622] e100: Copyright(c) 1999-2006 Intel Corporation
[ 1.599693] tlan: ThunderLAN driver v1.17
[ 1.604004] tlan: 0 devices installed, PCI: 0 EISA: 0
[ 1.681488] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.689524] davinci_mdio 4a101000.mdio: detected phy mask ffffffae
[ 1.698640] libphy: 4a101000.mdio: probed
[ 1.702962] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver unknown
[ 1.711348] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver unknown
[ 1.719809] davinci_mdio 4a101000.mdio: phy[6]: device 4a101000.mdio:06, driver unknown
[ 1.729840] cpsw 4a100000.ethernet: Detected MACID = f4:5e:ab:4d:ee:68
[ 1.736929] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.743653] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.749163] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.757615] cpsw 4a100000.ethernet: cpsw: Detected MACID = 64:69:4e:fc:82:cd
[ 1.766074] PPP generic driver version 2.4.2
[ 1.770832] PPP BSD Compression module registered
[ 1.775819] PPP Deflate Compression module registered
[ 1.781129] PPP MPPE Compression module registered
[ 1.786162] NET: Registered protocol family 24
[ 1.790847] PPTP driver version 0.8.5
[ 1.795041] usbcore: registered new interface driver asix
[ 1.800766] usbcore: registered new interface driver ax88179_178a
[ 1.807383] usbcore: registered new interface driver cdc_ether
[ 1.813562] usbcore: registered new interface driver cdc_eem
[ 1.819522] usbcore: registered new interface driver net1080
[ 1.825503] usbcore: registered new interface driver cdc_subset
[ 1.831754] usbcore: registered new interface driver zaurus
[ 1.837638] usbcore: registered new interface driver simcom_wwan
[ 1.843991] usbcore: registered new interface driver sierra_net
[ 1.850244] usbcore: registered new interface driver cdc_ncm
[ 1.856231] usbcore: registered new interface driver qmi_wwan
[ 1.863192] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.870032] ehci-platform: EHCI generic platform driver
[ 1.875776] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.882294] ohci-platform: OHCI generic platform driver
[ 1.888369] usbcore: registered new interface driver cdc_acm
[ 1.894328] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.902771] usbcore: registered new interface driver cdc_wdm
[ 1.908757] usbcore: registered new interface driver usb-storage
[ 1.915172] usbcore: registered new interface driver usbserial_generic
[ 1.922065] usbserial: USB Serial support registered for generic
[ 1.928385] usbcore: registered new interface driver ipw
[ 1.933994] usbserial: USB Serial support registered for IPWireless converter
[ 1.941515] usbcore: registered new interface driver option
[ 1.947376] usbserial: USB Serial support registered for GSM modem (1-port)
[ 1.954716] usbcore: registered new interface driver sierra
[ 1.960581] usbserial: USB Serial support registered for Sierra USB modem
[ 1.967742] usbcore: registered new interface driver usb_serial_simple
[ 1.974630] usbserial: USB Serial support registered for carelink
[ 1.981034] usbserial: USB Serial support registered for zio
[ 1.987019] usbserial: USB Serial support registered for funsoft
[ 1.993355] usbserial: USB Serial support registered for flashloader
[ 2.000032] usbserial: USB Serial support registered for google
[ 2.006276] usbserial: USB Serial support registered for libtransistor
[ 2.013152] usbserial: USB Serial support registered for vivopay
[ 2.019470] usbserial: USB Serial support registered for moto_modem
[ 2.026077] usbserial: USB Serial support registered for motorola_tetra
[ 2.033047] usbserial: USB Serial support registered for novatel_gps
[ 2.039723] usbserial: USB Serial support registered for hp4x
[ 2.045782] usbserial: USB Serial support registered for suunto
[ 2.052024] usbserial: USB Serial support registered for siemens_mpi
[ 2.061058] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc not found, using dummy regulator
[ 2.071573] am335x-phy-driver 47401300.usb-phy: Linked as a consumer to regulator.0
[ 2.082592] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 2.088456] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 2.096485] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 2.105176] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.112755] usb usb1: Product: MUSB HDRC host driver
[ 2.117953] usb usb1: Manufacturer: Linux 4.19.59-g5f8c1c6121 musb-hcd
[ 2.124801] usb usb1: SerialNumber: musb-hdrc.0
[ 2.130157] hub 1-0:1.0: USB hub found
[ 2.134212] hub 1-0:1.0: 1 port detected
[ 2.140129] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 2.150715] am335x-phy-driver 47401b00.usb-phy: Linked as a consumer to regulator.0
[ 2.161644] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 2.167515] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 2.175528] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 2.184219] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.191813] usb usb2: Product: MUSB HDRC host driver
[ 2.197011] usb usb2: Manufacturer: Linux 4.19.59-g5f8c1c6121 musb-hcd
[ 2.203859] usb usb2: SerialNumber: musb-hdrc.1
[ 2.209219] hub 2-0:1.0: USB hub found
[ 2.213271] hub 2-0:1.0: 1 port detected
[ 2.219824] omap_rtc 44e3e000.rtc: registered as rtc0
[ 2.225525] i2c /dev entries driver
[ 2.231904] cpuidle: enable-method property 'ti,am3352' found operations
[ 2.241123] usbcore: registered new interface driver usbhid
[ 2.247264] usbhid: USB HID core driver
[ 2.254159] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 2.260589] gre: GRE over IPv4 demultiplexor driver
[ 2.265928] Initializing XFRM netlink socket
[ 2.271161] NET: Registered protocol family 10
[ 2.277525] Segment Routing with IPv6
[ 2.281616] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.289276] NET: Registered protocol family 17
[ 2.294103] NET: Registered protocol family 15
[ 2.299382] can: controller area network core (rev 20170425 abi 9)
[ 2.306283] NET: Registered protocol family 29
[ 2.310950] can: raw protocol (rev 20170425)
[ 2.315504] can: broadcast manager protocol (rev 20170425 t)
[ 2.321906] 8021q: 802.1Q VLAN Support v1.8
[ 2.326355] lib80211: common routines for IEEE802.11 drivers
[ 2.332424] Key type dns_resolver registered
[ 2.337163] ThumbEE CPU extension supported.
[ 2.341721] Registering SWP/SWPB emulation handler
[ 2.346742] omap_voltage_late_init: Voltage driver support not added
[ 2.354471] Loading compiled-in X.509 certificates
[ 2.369587] OMAP GPIO hardware version 0.1
[ 2.376304] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 2.381841] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 2.389873] nand: device found, Manufacturer ID: 0xc2, Chip ID: 0xda
[ 2.396614] nand: Macronix MX30LF2G18AC
[ 2.400632] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 2.408665] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
请看下面工程师的回复。
USBx_DRVVBUS cannot be configured as GPIO, it won't work in USB mode.
Please try the following command to turn off the USB bus power:
This command is for USB1 controller. If USB0 controller is used, please replace 'musb-hdrc.1' with 'musb-hdrc.0'.