This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在新增.c文件后,编译报错:
LD StartApplication.out
Sh: ../../../tools/application-build/compiler/ti-cgt-arm_20.2.4.LTS/bin/armcl: Argument list too long
环境信息如下:
系统: Windows Server 2016 Standard
虚拟机: 否
SDK版本: 07_03_00_07
问题:是否可以通过修改编译选项的方式解决该问题?
After add .c file into project, compile error as following:
LD StartApplication.out
Sh: ../../../tools/application-build/compiler/ti-cgt-arm_20.2.4.LTS/bin/armcl: Argument list too long
Environment information is listed below:
Operation System: Windows Server 2016 Standard
VMWare : Not used
SDK version: 7.3.0.7
Question: Is it possible to solve the compile error with modifying compile options.
This thread is now created on the TI E2E global forum.
Closing the thread here.
Regards
Karan