HI:
We encountered the following problems debugging the mcspi driver using the MCUSW_01_03_03_02_CONFIG version:
1. We are currently using the default configuration mode (continue, sync mode), calling mcal's mcspi0 to send and read and write short data(likes read and peripheral register) is successful, but sending long data(over 16 bytes command data), through the waveform found that the data we sent is not the data we need, so we want to ask how to edit driver
2. We want to modify to (single, Async mode), but tried to modify the configuration, and according to the demo call spi driver failed, want to consult how to configure MCAL
3. We hope to add the DMA module in the future, but there is no way to configure it at present, do you have any relevant solutions or demos to help us solve it?
Thank you!