This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: USB 读写慢的问题。

Part Number: AM5708


我在使用AM5708 这款芯片的USB功能,挂载U 盘,测试读写速度的时候,发现读写速度很慢。

内核版本:4.9.28

下面是用 hdparm 工具测试的速度:

通过查看USB 可以看出 确实是2.0的读写速度。但是2.0的读写速度理论上来说应该是有,408Mbps。

测出来只有5Mbps,请问这个问题我需要从那个方向去排查呢?