This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: SPI flash boot 问题,生成的out文件过大,无法使用工具链进行转换

Part Number: TMS320C6678

尊敬的TI工程师您好:

参考C6678_SPIboot_usersManual.pdf 使用提供的led_play.out成功引导启动

但是自己的工程生成的out文件过大(在6M左右),在运行spiboot.bat执行到b2i2c led_play.btbl led_play.btbl.i2c这一步时

会提示报错Max input array size exceeded

将mcsdk_2_01_02_06\tools\boot_loader\ibl\src\util\btoccs路径下b2ccs.c和b2i2c.c源码中定义的#define SIZE 0x200000   /* max array size */修改后重新生成b2ccs.exe和b2i2c.exe

再次运行spiboot.bat不报错,但是生成的i2crom.ccs没有内容为0kb。

对 mcsdk_2_01_02_06\tools\boot_loader\ibl\src\util\romparse中的romparse.h文件下的#define MAX_DATA_LEN_32bit  32768进行修改后用MinGW重新生成romparse.exe但是生成的i2crom.ccs依旧为0kb,不知道是否需要修改别的地方。

另外有在e2echina.ti.com/.../evm6678le-i2c-nor-flash-boot-spi-flash-boot这篇帖子中看到有人提供了修改过的工具链,可以满足较大二进制文件的转换,但是我好像没有权限下载。