Part Number: TMS320C6655
环境: CCS 5.5, Complier: 8.3.12, DSP TMS320C6655
目标: 1. 理解DSP如何跳转到相应的Interrupt Service Routine; 2) 通过自己写代码来验证上述想法
在CCS中建立个工程,仅包含三个文件:main.c, intvecs.asm, and C665x.cmd (Linker Command File). 本人可以通过对ISR寄存器Bit4置位来触发INT4中断,随后IntDefaultHandler函数会被调用。但编译过程中报错,信息如下:
#10234-D unresolved symbols remain InterruptTest #10010 errors encountered during linking; "InterruptTest.out" not built InterruptTest unresolved symbol intcVectorTable, first referenced in ./main.obj InterruptTest
附上三个文件:
main.c
/*
* main.c
*/
#define C674X_NMI 1
#define C674X_GEE 2
#define C674X_XEN 3
#define C674X_INT_COUNT 16
#define NUM_SYS_EVENTS 128
extern cregister volatile unsigned int AMR; //Addressing mode register
extern cregister volatile unsigned int CSR; //Control status register
extern cregister volatile unsigned int GFPGFR; //Galois field multiply control register
extern cregister volatile unsigned int ICR; //Interrupt clear register
extern cregister volatile unsigned int IER; //Interrupt enable register
extern cregister volatile unsigned int IFR; //Interrupt flag register
extern cregister volatile unsigned int IRP; //Interrupt return pointer register
extern cregister volatile unsigned int ISR; //Interrupt set register
extern cregister volatile unsigned int ISTP; //Interrupt service table pointer register
typedef void (*c674xISR)(void);
void Intc_Init (void);
void IntDefaultHandler (void);
/******************************************************************************
** EXTERNALLY DEFINED FUNCTIONS
******************************************************************************/
extern void intcVectorTable(void);
/******************************************************************************
** STATIC VARIABLES/FUNCTIONS
******************************************************************************/
static c674xISR c674xISRtbl[C674X_INT_COUNT];
int main(void) {
Intc_Init();
// pInterruptRegs->INTMUX1 =
IER |= (1<<4) + (1<<1); // set INT4 and NMIE
CSR |= 1; // enable GIE
while(1)
{
ISR = (1<<4); // trigger INT4
asm(" NOP");
asm(" NOP");
asm(" NOP");
}
return 0;
}
void Intc_Init (void)
{
unsigned int step = 0;
/* Set ISRs to default "do-nothing" routine */
while(step != C674X_INT_COUNT)
c674xISRtbl[step++] = IntDefaultHandler;
/* Set interrupt service table pointer to the vector table */
ISTP = (unsigned int)intcVectorTable;
/* Clear pending CPU maskable interrupts (if any) */
ICR = 0xFFF0;
/* Enable NMIE bit to allow CPU maskable interrupts */
IER = (1 << C674X_NMI);
}
void Intc_IntRegister (unsigned int cpuINT, void (*userISR)(void))
{
/* Assign the user's ISR to the CPU maskable interrupt */
c674xISRtbl[cpuINT] = userISR;
}
/******************************************************************************
** INTERRUPT SERVICE ROUTINES - Used Internally
******************************************************************************/
void IntDefaultHandler (void)
{
while(1);
}
interrupt void c674x_nmi_isr (void)
{
c674xISRtbl[1]();
}
interrupt void c674x_rsvd_int2_isr (void)
{
c674xISRtbl[2]();
}
interrupt void c674x_rsvd_int3_isr (void)
{
c674xISRtbl[3]();
}
interrupt void c674x_mask_int4_isr (void)
{
c674xISRtbl[4]();
}
interrupt void c674x_mask_int5_isr (void)
{
c674xISRtbl[5]();
}
interrupt void c674x_mask_int6_isr (void)
{
c674xISRtbl[6]();
}
interrupt void c674x_mask_int7_isr (void)
{
c674xISRtbl[7]();
}
interrupt void c674x_mask_int8_isr (void)
{
c674xISRtbl[8]();
}
interrupt void c674x_mask_int9_isr (void)
{
c674xISRtbl[9]();
}
interrupt void c674x_mask_int10_isr (void)
{
c674xISRtbl[10]();
}
interrupt void c674x_mask_int11_isr (void)
{
c674xISRtbl[11]();
}
interrupt void c674x_mask_int12_isr (void)
{
c674xISRtbl[12]();
}
interrupt void c674x_mask_int13_isr (void)
{
c674xISRtbl[13]();
}
interrupt void c674x_mask_int14_isr (void)
{
c674xISRtbl[14]();
}
interrupt void c674x_mask_int15_isr (void)
{
c674xISRtbl[15]();
}
intvecs.asm
;
; File: intvecs.asm
;
; Brief: Contains interrupt vector table and fetch packets
;
; Copyright (C) 2011 Texas Instruments Incorporated - http://www.ti.com/
; ALL RIGHTS RESERVED
;**********************************************************
; Global Symbols
;**********************************************************
.global _intcVectorTable
.ref __c_int00
.global _c674x_nmi_isr
.global _c674x_rsvd_int2_isr
.global _c674x_rsvd_int3_isr
.global _c674x_mask_int4_isr
.global _c674x_mask_int5_isr
.global _c674x_mask_int6_isr
.global _c674x_mask_int7_isr
.global _c674x_mask_int8_isr
.global _c674x_mask_int9_isr
.global _c674x_mask_int10_isr
.global _c674x_mask_int11_isr
.global _c674x_mask_int12_isr
.global _c674x_mask_int13_isr
.global _c674x_mask_int14_isr
.global _c674x_mask_int15_isr
;**********************************************************
; Interrupt Fetch Packet
;**********************************************************
VEC_ENTRY .macro addr
STW B0,*--B15
MVKL addr,B0
MVKH addr,B0
B B0
LDW *B15++,B0
NOP 2
NOP
NOP
.endm
;**********************************************************
; Interrupt Vector Table
;**********************************************************
.align 1024
_intcVectorTable:
VEC_ENTRY __c_int00
VEC_ENTRY _c674x_nmi_isr
VEC_ENTRY _c674x_rsvd_int2_isr
VEC_ENTRY _c674x_rsvd_int3_isr
VEC_ENTRY _c674x_mask_int4_isr
VEC_ENTRY _c674x_mask_int5_isr
VEC_ENTRY _c674x_mask_int6_isr
VEC_ENTRY _c674x_mask_int7_isr
VEC_ENTRY _c674x_mask_int8_isr
VEC_ENTRY _c674x_mask_int9_isr
VEC_ENTRY _c674x_mask_int10_isr
VEC_ENTRY _c674x_mask_int11_isr
VEC_ENTRY _c674x_mask_int12_isr
VEC_ENTRY _c674x_mask_int13_isr
VEC_ENTRY _c674x_mask_int14_isr
VEC_ENTRY _c674x_mask_int15_isr
C665x.cmd
-stack 0x4000
-heap 0x4000
MEMORY
{
L2SRAM o = 0x00800000 l = 0x00100000 /* 1MB L2SRAM */
/* Core0 running IBL will take up 0x0C000000 ~ 0x0C01FFFF(128KB), reserve at here! */
MSMCSRAM o = 0x0C010000 l = 0x000F0000 /* 896KB MSMCSRAM */
DDR3 o = 0x80000000 l = 0x20000000 /* 512MB DDR3 */
//MSMCRAM o = 0xC000000 l = 0x00100000
}
SECTIONS
{
.text > L2SRAM
.cinit > L2SRAM
.const > L2SRAM
.switch > L2SRAM
.stack > L2SRAM
.fardata > L2SRAM
.cio > L2SRAM
.far > L2SRAM
GROUP
{
.neardata /* far uninitialized global and global variables */
.rodata /* global static constant */
.bss /* uninitialized global variables*/
} > L2SRAM
}
看上去intvecs.asm未被编译,导致main.c无法识别全局变量intcVectorTable。
查阅了很多资料和论坛帖子,至今未解决。请TI专家识别下哪里有缺失。万分感谢。