This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678连接时出错



我们使用的仿真器是560V2USB,运行的是最为基础的helloworld 程序,在built 完成之后,Debug 的过程中(约在进度96%的位置)报错,报错内容为:error initialing emulator。此时评估版上的指示等并未闪烁,只有电源指示灯是亮的,看起来仿真器并未链接成功。

同时,从TI公司配带的光盘安装系统,并未能找到evmc6678.gel文件,请工程师上传一个。

另外就是使用X100V1 USB仿真器时,找不到6678的设备,是否缺少文件?

十分感谢!!

  • 在工作的过程中,发现了新的问题,在使用560V2USB进行仿真加载时,电源指示灯是亮的,其余的不亮,是否是硬件问题,SW3-6的DIP开关均按要求设置。

    另外,在使用X100V1进行链接时,Lanuch能够成功,单在链接Core时,显示 error connection to target, can't acess to the rigister &2…………,请问,这又是为什么呢,难道又是电路问题,刚买的评估版,不该出现这么多问题呀。

  • Wei Jia 你好!

    CCS报错的原因可能是由于你在操作的过程中出现了错误。

    Target board上电后不要立即在板子上跑工程,稍微等待几秒钟。

    使用XDS100v1 USB emulator时是可以找到c6678的设备的,请再次确认。

    正确的做法是:

    1、Build你所建的工程,编译和链接后生成.out文件;

    2、Launch Target文件,文件的配置是:Connection选项请选择Blackhawk XDS560v2-USB Mezzanine Emulator,Board or Device请选择TMSC6678,然后在Advanced选项卡中将c66x_0的Initialization script填入c6678的gel文件,gel文件的路径为:C:\Program Files\Texas Instruments\ccsv5\ccs_base\emulation\boards\evmc6678l\gel;

    3、将生成的.out文件Load到你需要跑这个工程的core上;

    4、Run你所建立的工程。

    请按照上述过程操作一遍,如果任然有问题,欢迎与我们再联系。

    evmc6678l.gel
  • 我会按照上述做法再做一遍,谢谢