This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6655: Wireshark捕获不到第一帧Ethernet数据

Part Number: TMS320C6655

环境:CCS5.5, Win11 64 bits(未使用CSL库,所有寄存器操作都是通过自行编程完成)

硬件环境:C6655+PHY 88E1112,对端是10M/100M自适应网卡,并用Wireshark捕捉该网卡数据。

问题:DSP通过发送通道0发送一帧数据,Wireshark没有捕捉到,但TXINTSTATRAW第0位置位。

调查进展:初始化过程中,读取MR_LP_ADV_ABILITY寄存器,已经识别到SGMII的模式为100M全双工,同时Link已经Up。随后初始化EMAC寄存器,配置发送数据描述符Descrptor,随后放入HDP0进行发送,TXINTSTATRAW第0位置位,但Wireshark未捕捉到。在TX0CP中写入EMAC处理的Descriptor地址,TXINTSTATRAW第0位清零。

从调查的结果来看,看上去EMAC已经处理了通道0的发送数据,而且接受了achknoledge(CP寄存器操作)。MAC Control Register配置成0x00040221: EXT_EN, TX_PTYPE, GMII_EN Transmit Pacing Enable, FULLDUPLEX 这4个bit置位。

请TI专家帮忙看看为何Wireshark没有捕捉到数据呢