我用的是AM3359处理器,把一个opt压缩文件拷到文件系统里面,解压缩之后出现这个问题:
opt/Qt4.8.1/lib/libQtGui.la
opt/Qt4.8.1/lib/libQtGui.so.4
opt/Qt4.8.1/lib/libQtGui.so.4.8.1
[ 112.087463] UBI error: ubi_io_write: error -5 while writing111 2048 bytes to PEB 1586:108544, written 0 bytes
[ 112.097991] UBI warning: ubi_eba_write_leb: failed to write data to PEB 1586
[ 112.105468] UBI: recover PEB 1586, move data to PEB 5531
[ 112.124694] UBI error: ubi_io_write: error -5 while writing111 512 bytes to PEB 5531:2048, written 0 bytes
[ 112.134918] UBI warning: recover_peb: failed to write to PEB 5531
[ 112.141326] UBI: try again
[ 112.144226] UBI: recover PEB 1586, move data to PEB 5532
[ 112.150512] UBI: run torture test for PEB 5531
[ 112.175964] UBI error: ubi_io_write: error -5 while writing111 512 bytes to PEB 5532:2048, written 0 bytes
[ 112.186187] UBI warning: recover_peb: failed to write to PEB 5532
[ 112.192626] UBI: try again
[ 112.195495] UBI: recover PEB 1586, move data to PEB 5533
[ 112.301269] UBI error: ubi_io_write: error -5 while writing111 131072 bytes to PEB 5531:0, written 0 bytes
[ 112.311523] UBI error: erase_worker: failed to erase PEB 5531, error -5
[ 112.318511] UBI: reserve more 1 PEBs
[ 112.322296] UBI: mark PEB 5531 as bad
[ 112.339813] UBI: 81 PEBs left in the reserve
[ 112.370269] UBI: run torture test for PEB 5532
[ 112.405151] UBI error: ubi_io_write: error -5 while writing111 106496 bytes to PEB 5533:4096, written 0 bytes
[ 112.415679] UBI warning: recover_peb: failed to write to PEB 5533
[ 112.422088] UBI: try again
[ 112.424987] UBI: recover PEB 1586, move data to PEB 5534
[ 112.443939] UBI error: ubi_io_write: error -5 while writing111 512 bytes to PEB 5534:2048, written 0 bytes
[ 112.454132] UBI warning: recover_peb: failed to write to PEB 5534
[ 112.460571] UBI warning: ubi_ro_mode: switch to read-only mode
[ 112.466766] UBIFS error (pid 865): ubifs_leb_write: writing 2048 bytes to LEB 1514:104448 failed, error -5
[ 112.476928] UBIFS warning (pid 865): ubifs_ro_mode: switched to read-only mode, error -5
[ 112.485473] Backtrace:
[ 112.488098] [<c0018a54>] (dump_backtrace+0x0/0x108) from [<c042ab4c>] (dump_stack+0x18/0x1c)
[ 112.497009] r6:00019800 r5:cf0a1000 r4:fffffffb
[ 112.501892] [<c042ab34>] (dump_stack+0x0/0x1c) from [<c017f634>] (ubifs_ro_mode+0x6c/0x78)
[ 112.510620] [<c017f5c8>] (ubifs_ro_mode+0x0/0x78) from [<c0180598>] (ubifs_leb_write+0xf8/0x1
求大神!!!