This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: 加密型TMS320 C6748芯片如何解锁JATG口进行DSP程序下载

Part Number: TMS320C6748

以前一直使用的是TMS320C6748芯片,这一次采购的时候只有带E的加密型TMS320C6748 E芯片,使用CSS11.0和XDSV2下载器,在连接JATG口对DSP程序进行下载时报错:C674X_0: Error connecting to the target: (Error -6311) PRSC module failed to write to a register. (Emulation package 9.7.0.00213),也查阅了论坛相关帖子,问题在加密型芯片下载之前需要使用工具烧录一个.bin文件将JATG口解锁。可能是其他帖子的时间都较早以前,里面给的wiki的连接目前链接到的是芯片的具体使用手册,我也较为详细的阅读了手册,其中并没有发现有关如何解锁JATG口的方法,同时手册中第三页中关于该系列芯片安全使用手册的链接也已经失效。

所以,想向各位寻求解锁JATG口的工具,对应的.bin文件以及较为详细的解锁操作过程,

谢谢大家,有不对的地方请多指教