大家好,目前使用AM3354的网口进行网络数据分析使用。硬件接法是设备A----交换机-----设备B,然后交换机---AM3354的网口(RMII接口外扩PHY和变压器后连接),设置交换机的镜像功能,这样可以将设备A/B通信数据镜像到AM3354对应的网口上面采集,从而分析设备A和B的通信问题。
现在的问题是,AM3354的网口可以正常接收A/B之间的广播ARP数据,但是AB之间通信的UDP数据,就是不进AM3354的网口接收中断,从而无法接收UDP数据。
1、通过电脑网口代替AM3354网口,是可以接收到UDP的镜像数据的,说明交换机镜像功能正常。
2、AM3354的网口可以接受到ARP广播数据,说明网口接收数据正常,可以进入接收数据完成中断;
3、A/B正常通信时,用示波器测试AM3354的RMII的RXD0/1信号线也可以采集到波形数据,A/B端口时刚好也没有波形,也能证明镜像数据已经转接到RMII接口了。
4、单测试AM3354的网口通信收发功能正常,也没有问题。
但是现在问题就是,UDP数据不进AM3354的中断,请大家帮忙分析一下还可能是哪块的原因?谢谢