Other Parts Discussed in Thread: TDA4VM,
各位老铁们,关于TDA2系列芯片大概有多少算力的问题,有咨询过TI的官方,给出的解释是每个TDA2的芯片的算力是不太相同的,需要去算具体的算法如下:
Q; Client want to know how many DMIPS and TOPS does the TDA2 and TDA3 have.
A:
There are multiple parts. you can compute TOPS based upon which part are you looking and instances of C6x DSP and EVEs.
Each C6x DSP has 32 MACs/cycle for 8 bit and 16 bit data type
Each EVE has 16 MACs/cycle for 8bit and 16 bit data type
For example a device with 1 EVE @650 MHz and 1 C6x DSP@750 MHz have 16*650M + 32*750M = 34.4 GMACS = 68.8 GOPS
Typically these are older devices and will have fraction of TOPS. For higher TOPS devices you should refer TDA4x parts. For example TDA4VM has 8 TOPS.
本以为这个问题快速解决了,但是在具体计算中遇到了难题,芯片手册没有找到具体的一些计算支持信息,就如TDA2eg-17为例:

没有具体的一些信息,使用公式计算失败,所以老铁们是如何计算的呢,感觉仅仅有手册是不够的,还需要什么资料来做支撑,感谢老铁们!
PS:我从别人了解到TDA2S芯片的大概算力是0.4TOPS,是不是TDA2这个系列的算力都差不多呢,或者这个系列的算力大概是多少???