This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: 网口link通,但是ping不通

Part Number: TMS320C6678

自制板,基于NDK例程(helloworld)进行修改测试百兆网。

使用的是SGMII0口,在程序中已修改为初始化port0,现在的情况是link可以通,然后打印信息如下,但是ping不通。请问这可能是因为什么呢?

[C66xx_8] QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized

TCP/IP Stack 'Hello World!' Application


TCP/IP Stack 'Hello World!' Application

PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.0.11