This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: 摄像头Trigger信号等问题

Part Number: TDA4VM-Q1


Dear TI support,

我们正在做TDA4AL的开发,有几个问题还请帮忙解答:

1、HS芯片内部的OTP用户侧可读么?还是完全由DMSC控制,用户侧不可见?

2、芯片的ID是指如下寄存器内值么?ID是否是每颗TDA4独立且唯一的?TRM里面对应地址位为4300 0020h~4300 002Ch?

3、我们想由TDA4提供双目camera 外部触发信号(Trigger),并且能精确调整两个trigger信号之间的delay,最好能到us级别,我们应该把trigger信号连到支持timer的IO上么?如果是,应该放在MCU域的timer还是main 域的timer上?

4、我在哪里能看到TDA4AL详细的order信息?

5、是否有芯片的功耗评估工具?比如每路电大概的电流值。

6、是否有硬件设计checklist?