This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: SPI启动模式时,bootmode[12:10]的值如何设计,如何解决与PLL设置的冲突

Part Number: TMS320C6657

工程师您好!

我们现在使用C6657进行设计,从SPI进行启动,此时需要用到bootmode[12:10],我们需要的是000;

但同时这三bit也是PLL的设计,外部时钟是100MHz,则是011;

请问这个冲突是要如何解决?

感谢!