This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: AM5708中imglib.ae66的编译问题

Part Number: AM5708

TI的技术支持工程师:
您好!我正在使用AM5708,最近遇到一个问题。我想使用imglib.ae66库中的IMG_sobel_3x3_8算子进行sobel边缘检测,目前使用没问题,可以正常检测图像边缘。但是原函数接口没有输出X方向和Y方向的梯度值,而我自己在IMG_sobel_3x3_8.h和IMG_sobel_3x3_8.c中对函数实现进行了修改,增加了X方向和Y方向的梯度值的输出,但是发现不知道怎么把它重新编译到imglib.ae66库中。我想知道到底能不能重新编译imglib.ae66库?如果可以编译,那么编译方法是什么?我在Linux系统下,路径为" .../ti-processor-sdk-linux-rt-am57xx-evm-04.03.00.05/linux-devkit/sysroots/armv7ahf-neon-linux-gnueabi/usr/share/ti/ti-imglib-c66x-tree/packages/ti/imglib/src/IMG_sobel_3x3_8"。如果不能重新编译,我只有自己把原函数代码拷贝出来再修改,把它作为自己创建的一个函数,然后使用OPENCL进行调用了,这样估计也可以,就是麻烦一点。希望能得到您的帮助!