This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

b2i2c工具问题(关于创建由SPI norflash直接加载的镜像)



你好:

    我们用的EVM板子是6670的, 想通过SPI NORFLASH直接加载. 我们尝试根据Andy Yin给的"SPI boot"的例程"spiboot.bat"的步骤对CCSv5.3生成的.out文件进行操作.第一步能通过hex6x的工具成功转换为btbl的格式.到了第二步要用b2i2c工具转换成.btbl.i2c格式的时候,b2i2c提示"Max input array size exceeded".我们用的.out文件大小为2,614KB,生成的.btbl文件大小为632KB.

    问题:

1)b2i2c工具对于文件输入是否有大小限制?如有,限制的大小是多少?对于该情况该如何操作?我的操作是否有误?谢谢!

2)经过"spiboot.bat"的步骤后,我们是否可以得到直接烧到norflash的文件并实现由SPI Norflash直接加载?

3)"spiboot.bat"文件的步骤是否正确?附上"spiboot.bat"文件

Karlphy

祝工作顺利!