This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 软件中如何实现每个核任务独立?

6678编程时如果实现每个核的任务独立,或者说每个核有对应的一个main函数吗?

  • 6678多核之间本来就是独立关系,每个核运行自己的main函数。

  • 是否方便传一下简单的例程,非常感谢,正在考虑入手6678板

  • 下面是一个简单的多核启动的例子(core0触发core1~core7的执行),你可以作为参考:

    #include <stdio.h>
    #include <stdlib.h>
    #include <string.h>


    #define BOOT_MAGIC_ADDRESS 0x0087FFFC
    #define GLOBAL_ADDR(addr, corenumber) (unsigned int)addr<0x1000000?\
          (unsigned int)addr+(0x10000000+corenumber*0x1000000):\
          (unsigned int)addr

    extern far unsigned int _c_int00;

    int a = 1;
    int b = 2;
    int c;

    void main(void) {
     
     int coreNumber;
     unsigned int * bootMagicAddr;
     unsigned int bootEntryAddr;
     //unsigned int entry = 0x0c0095a0; // address of "_c_int00", read from *.map file
     char str[256];

     // get DSP core number
     unsigned int DNUM = ((*((volatile unsigned int *)(0x01840000))) & 0x000F0000) >> 16;

     // output
     c = a + b;
     printf(str); // printf in CCS


     // core0 try to wake up other cores
     if(DNUM == 0)
     {
      kicker_unlock();
      for(coreNumber = 1; coreNumber < 8; coreNumber++)
      {
       // set maggic address of core(coreNumber)
       bootMagicAddr = (unsigned int *)(GLOBAL_ADDR(BOOT_MAGIC_ADDRESS, coreNumber));
       bootEntryAddr = GLOBAL_ADDR((&_c_int00), coreNumber);
       *bootMagicAddr = bootEntryAddr;

       // generate IPC to core(coreNumber)
       *((volatile unsigned int *)(0x02620240 + (coreNumber * 4))) = 1;

       delay(10000000);
      }
      kicker_lock();
     }

    }

    当多核执行同一个程序时,即用DNUM来区分当前执行程序的是哪个核。例如:

    switch(DNUM)

    {

    case 0:

        func0();

        break;

    case 1:

        func1();

        break;

    case 2:

        func2();

        break;

    case 3:

        func3();

        break;

    case 4:

        func4();

        break;

    case 5:

        func5();

        break;

    case 6:

        func6();

        break;

    case 7:

        func7();

        break;

    default;

        break;

    }

  • 最近就在搞这个,首先非常感谢看到你的回复,还想请问一下您:

    上述例子程序是把所有8个核的程序放在一个工程中,然后用核心号分辨是哪个核的对吗?也就是说最终只生成一个.out文件,然后首先boot到核0,由核0用上述代码给其他核加载是吧?

    您有没有相关的简单的例子程序能给我发一下吗?