This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,TI
我遇到了一个关于1080p分辨率的问题,是在ipnc4.0开发包里面调试的。我需要得到1920*1080的图像,RAW数据的分辨率是1920*1088,但是经过编码之后,输出的图像数据就变成1920*1072。通过查找,发现图像在编码的时候,宽高被这样子操作了:
config->encodeConfig[i].cropWidth = ALIGN_ENCODE(1920);
config->encodeConfig[i].cropHeight = ALIGN_ENCODE(1080);
这两句的意思是,16对齐,于是1920*1080就变成了1920*1072;
为了使得编码之后的图像为1920*1080,我使其8对齐,这样就是1920*1080,但是图像底部又有一些跳动。
我该从何处下手呢?
16字节对齐,1088不会被截断成1072吧?你把原代码改成
config->encodeConfig[i].cropWidth = ALIGN_ENCODE(1920);
config->encodeConfig[i].cropHeight = ALIGN_ENCODE(1088);
然后再看结果。
谢谢 Robin Edson的回答,但是我的目标不是8对齐,还是16对齐;
不关源程序怎么处理,如果是8对齐,那么1088是符合条件的,如果是16对齐,同样1088也满足条件;
因为源程序是lib的形式存在,所以只要保证给参数符合它的要求,就ok,否则就是bug。你说是不是呢?
可能我的问题没有写清楚,不知道你对TI的H264是否熟悉,我比较纳闷为什么在TI的H264的指导手册里面规定输入帧的高、宽必须是16位?
目前我想获取1920*1080的图像,该如何整呢?