This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

beaglebone black的uboot改1024 600 16bit位宽寄存器修改问题



我用了beaglebone black的7" 1024 600的cape

原先的uboot和linux都是24bit的lcd输出,linux下我改了输出为16bit成功的

但uboot下面我根据暑假手持修改寄存器

am335x 16bit tft 输出模式设置:
RASTER_CTRL[9, 7, 1]   Active (TFT) Color 16       x10
16 BPP in active mode (LCDTFT = 1 and TFT24 = 0 in RASTER_CTRL)
屏幕却乱闪
不知道有无什么齐其他寄存器需要修改?