This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm distclean
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm ti8168_dvr_min_sd
make CROSS_COMPILE=arm-none-linux-gnueabi- ARCH=arm u-boot.ti
经过编译后生成 u-boot.bin和u-boot.noxip.bin两个文件,将u-boot.noxip.bin重命名为MLO后,将u-boot.bin和MLO都复制到SD卡中,但是运行不起来。
是否还需要配置别的,我的开发板是dm8168_dvr的。
加载到1GB的ddr板子上时,出现如下信息起不来:
Rules.make里面DDR_MEM是DDR_MEM_1024M还是DDR_MEM_2048M??
。。 这种编译的错误除了别人正好碰到之外,只能自己调试找原因啊,
如果别人都没碰到过只能建议你找台机器重新解压缩包看一下,
另外你好好check Rules.make里面的配置吧。比如说你的board type是选了dvr 不是evm吧