This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8168 u-boot ddr

想问一下,1GB的ddr已经正常运行,在配置2GB的DDR的时候,是否将Rules.make文件中的DDR_MEM=DDR_MEM_2048M就可以了!

  • 再注意下内存空间分配和硬件版本应该没什么问题

  • 内存空间分配使用的是那个文件啊!dm8168_dvr!

  • dvr_rdk的Rules.make 配置了DDR_MEM=DDR_MEM_2048M   不就是加载config_2G.bld

  • The memory map of complete DVRRDK is controlled in <DVR_RDK>/dvr_rdk/mcfw/src_bios6/cfg/ti81<x>x/config_<xxxx>.bld

    In this build configuration file, size of each section can be reconfigured. For example, in config_1G_256M.bld, DSP code size and DSP data size section can be changed by modifying the following entries. DSP_CODE_SIZE = 1*MB + 1*MB/2; DSP_DATA_SIZE = 13*MB;

    The base addresses of each section are incremented based on the base address of previous section and the size of the previous section. For example, if sections are created in the numerical order, base address of Section 2 is calculated as below: <Start Addr of Sect 2> = <Start Addr of Sec 1> + <Size of Sect 1>

x 出现错误。请重试或与管理员联系。